EIO0000005081.01

Serial Interface (COM on Box Module)

Introduction

The serial interface is not isolated. The SG (signal ground) and FG (frame ground) terminals are connected inside this product. When the serial interface connector is D-Sub, connect the FG wire to the shell.

DANGER
ELECTRIC SHOCK AND FIRE
When using the SG terminal to connect an external device to this product:
  • Verify that a ground loop is not created when you set up the system.
  • Connect the SG terminal to remote equipment when the external device is not isolated.
  • Connect the SG terminal to a known reliable ground connection to reduce the risk of damaging the circuit.
Failure to follow these instructions will result in death or serious injury.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use a D-Sub 9 pin connector that has jack screws.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

RS-232C

D-Sub 9 pin plug connector

Product side:

Pin No.

RS-232C

Signal name

Direction

Description

1

CD

Input

Carrier detect

2

RD (RXD)

Input

Receive data

3

SD (TXD)

Output

Send data

4

ER (DTR)

Output

Data terminal ready

5

SG

-

Signal ground (not isolated)

6

DR (DSR)

Input

Data set ready

7

RS (RTS)

Output

Request to send

8

CS (CTS)

Input

Send possible

9

CI (RI)

Input

Called status display

Shell

FG

-

Frame ground (common with SG)

Recommended jack screw is #4-40 (UNC).

RS-422/485

D-Sub 9 pin plug connector

Product side:

Pin No.

RS-422/485

Signal name

Direction

Description

1

RDA

Input

Receive data A (+)

2

RDB

Input

Receive data B (+)

3

SDA

Output

Send data A (+)

4

ERA*1

Output

Data terminal ready A (+)

5

SG

-

Signal ground (not isolated)

6

CSB*1

Input

Send possible B (-)

7

SDB

Output

Send data B (-)

8

CSA*1

Input

Send possible A (+)

9

ERB*1

Output

Data terminal ready B (-)

Shell

FG

-

Frame ground (common with SG)

*1 In RS-422, these control signals are available only when HMI mode is selected in UEFI BIOS. Refer to Settings of Serial Interfaces on Box Module.

Recommended jack screw is #4-40 (UNC).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.