EIO0000005081.01

Searching for the Manual

The following describes how to search for the Trellix software manual. Check the software version beforehand.
  1. Select the Settings button.
  2. Select App.
  3. In Apps & features, select Trellix Solidifier.
  4. Confirm the version.
  5. Close the App screen.
  6. Display https://docs.trellix.com/bundle in the web browser.
  7. Search for the corresponding manual for the supported version of McAfee Application Control.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.