EIO0000005081.01

Front USB

Enables/disables the front USB port on the Display Module.

Default: Off (Disable)

NOTE:
  • If the front USB is enabled, the risk of unauthorized access and infection of malicious software increases. Disable the front USB after use.

  • In models without a front USB port, this setting is disabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.