EIO0000005081.01

Accessories

Products may change or be discontinued without notice. Please check our website for the latest information.
www.se.com/docs

Product name

Product number

Interfaces

M.2 RS-232C isolated x 2

HMIYP6M2R23P2

M.2 RS-422/485 isolated x 2

HMIYP6M2R42P2

M.2 Ethernet (GbE IEEE1588) x 1

HMIYP6M2ETH

4G Cellular for Global

HMIYP6M24GW

M.2 WiFi/Bluetooth

HMIYP6M2WF

Storage

M.2 SSD 128 GB (Standard Endurance)

HMIYP6M2128L

M.2 SSD 128 GB (High Endurance)

HMIYP6M2128

M.2 SSD 256 GB (High Endurance)

HMIYP6M2256

M.2 SSD 512 GB (High Endurance)

HMIYP6M2512

SD Memory Card 64 GB

HMIYP6SD64GCX

Memory

DIMM 4 GB

HMIYP6DM4

DIMM 8 GB

HMIYP6DM8

DIMM 16 GB

HMIYP6DM16

Cables

4G Cellular extended antenna cable 3 m (2 pieces)

HMIYP6CB4G3M

WiFi/Bluetooth extended antenna cable 3 m (2 pieces)

HMIYP6CBWF3M

USB Front Cable

XBTZGUSB

Adapters

Book mount adapter for Basic Box (2 pieces for side mounting)

HMIYP6ADBMB

Panel cutout adapter for HMIDT752 (15" Wide)*2

HMIZHAT7W1

Panel cutout adapter for HMIDT952 (19" Wide)*2

HMIZHAT8W1

Panel cutout adapter for Harmony iPC S-Panel PC (10" Wide)*2

HMIZPAT5W1

Panel cutout adapter for Harmony iPC Modular Panel PC (12" Wide)*2

HMIZPAT6W1

Panel cutout adapter for Harmony iPC Modular/S-Panel PC (15" Wide)*2

HMIZPAT7W1

Panel cutout adapter for Harmony iPC Modular/S-Panel PC (19" Wide)*2

HMIZPAT8W1

Panel cutout adapter for Harmony iPC Modular Panel PC (22" Wide)*2

HMIZPAT9W1

Screen sheets

Anti-glare sheet for 10" Wide (5 sheets/set)

HMIZCAG5W1

Anti-glare sheet for 12" Wide (5 sheets/set)

HMIZCAG6W1

Anti-glare sheet for 15" Wide (5 sheets/set)

HMIZCAG7W1

Anti-glare sheet for 19" Wide (5 sheets/set)

HMIZCAG8W1

Anti-glare sheet for 22" Wide (5 sheets/set)

HMIZCAG9W1

Screen protection sheet for 12" (5 sheets/set)

HMIZG66

Screen protection sheet for 15" (5 sheets/set)

MPCYK50SPSKIT

Others

M.2 cooling kit for Basic Box*3

HMIYP6HSM2B

Trellix license

HMIYP6LSMCA

Recovery USB for Basic Box

HMIYP6RUSW10B

USB Clamp Type A (5 pieces/set)

HMIZCCLUSA

USB Clamp Type C (5 pieces/set)

HMIYP6CLUSC

*1 This is a passive cable.

*2 The range for the allowable panel thickness varies depending on the panel cut adapter. For information, refer to the panel cut adapter instruction manual.

*3 Required when installing M.2 SSD.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.