EIO0000005081.01

In-Band ECC

The CPU in this product supports In-Band ECC. The following describes the procedure for enabling and disabling In-Band ECC (default: Disabled).

  1. Display the BIOS screen. Refer to UEFI BIOS Setup Menu.

  2. Select Advanced > CPU Configuration > In-Band ECC.

  3. Select Enabled or Disabled.

  4. Press the [F4] key.

  5. Select Yes in the Save & Exit Setup dialog box.

  6. The product is restarted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.