EIO0000005081.01

Book Mounting

Book mounting requires an optional book mount adapter.

Book mount adapter for Basic Box: HMIYP6ADBMB

Installation procedure

  1. When attaching the side of the Box Module to the panel, use A.
  2. Remove the screws attached to the product (4 pieces), then fix the book mount adapter with the screws to attach it to the product.
    NOTE:
  3. Install the product to the panel or wall with M4 screws (4 pieces).
    NOTE:
    • The necessary torque is 1.5 N•m (13.3 lb-in).

    • When installing on the side of the product, the interface side (the bottom of the product) must be facing downward.

    • To prevent abnormally high temperatures from occurring inside the product, mount the product completely vertically.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.