EIO0000005081.01

How to Run System Monitor

This product comes with our original system monitor–a dashboard created with Node-RED. You can run the system monitor from the System Monitor icon in the Launcher.

The first time System Monitor is started, the Microsoft Edge settings screen will appear. The Windows Security Alert screen will also appear. Select Allow access if you allow other computers on the network to use the dashboard; select Cancel if you do not.

NOTE: When deciding whether to allow access, keep security under careful consideration.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.