EIO0000005081.01

System Backup

After product setup, backing up the system is recommended. Prepare a commercially available USB memory with a size of 32 GB or more, to create a backup USB.

NOTE: When HORM is enabled or immediately after hibernation, system backup or recovery will not run properly. Perform system backup or recovery after first disabling HORM and then shutting down the product.
Creating the backup USB
  1. Prepare a commercially available USB memory.
  2. Use the Recovery USB Creation Tool to create a recovery USB. Download the Recovery USB Creation Tool from the following URL and create a recovery USB by following the instructions on the website.
    www.se.com/ww/en/download
  3. Insert the recovery USB created with the Recovery USB Creation Tool into the product.
  4. Turn on the product.
  5. While the boot screen is displayed, press the [F7] key.
  6. Enter the password (default password: Pw#12345).
  7. From the following screen, select the recovery USB.
  8. Select Backup > OK.
  9. Select the disk to backup. Only C drive can be backed up. If several storage devices are shown in the dialog box, select the storage device of C drive. If there is only one storage device, the following screen does not appear and skip to step 10.
  10. Select the drive labeled "Other label", enter a file name, and select either Save or Open.
  11. In the confirmation screen, select OK.
  12. Backup begins.
  13. After backup is complete, the following screen is displayed. Remove the backup USB from the product, and then select Restart or Shutdown.

    To restore the system, refer to System Recovery.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.