EIO0000005081.01

Maintenance Accessories

Product name

Product number

Display Module

12-inch Display Module

HMIDM6600TM*1

15-inch Display Module

HMIDM6700TM*1

10-inch Wide Display Module

HMIDM6500WC*1

12-inch Wide Display Module

HMIDM6600WC*1

15-inch Wide Display Module

HMIDM6700WC*1

19-inch Wide Display Module

HMIDM6800WC*1

22-inch Wide Display Module

HMIDM6900WC*1

Installation gaskets

Installation gasket for 12" (1/set)

HMIZD56

Installation gasket for 15" (1/set)

HMIZD57

Installation gasket for 10" Wide (1/set)

HMIZD55W

Installation gasket for 12" Wide (1/set)

HMIZD56W

Installation gasket for 15" Wide  (1/set)

HMIZX57W

Installation gasket for 19" Wide (1/set)

HMIZCWG8W1

Installation gasket for 22" Wide (1/set)

HMIZCWG9W1

Installation fastener (4 pieces/set)

HMIZCAF1

Power connector (DC) (5 pieces/set)

HMIZCCNDC1

*1 Includes models ending with additional characters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.