EIO0000005081.01

Package Contents

This product has been carefully packed with special attention to quality. However, should you find anything damaged or missing, please contact your local distributor immediately.

Box Module

Verify all items listed here are present in your package:

  1. Harmony P6 Basic Box x 1

  2. USB cable clamp (Type A) x 2 sets (2 clips and 2 ties)

  3. USB cable clamp (Type C) x 1 set (1 clip and 1 tie)

  4. DC Power connector x 1

  5. M4 screws x 4 (to install the Display Module)

Panel Type

Verify all items listed here are present in your package:

  1. Harmony P6 Basic Model x 1

  2. Installation gasket (attached to this product) x 1

  3. Installation fasteners (to install on a panel):

    4 pieces (for 12-inch, 10-inch Wide and 12-inch Wide models)

    8 pieces (for 15-inch, 15-inch Wide, 19-inch Wide and 22-inch Wide models)

  4. USB cable clamp (Type A) x 2 sets (2 clips and 2 ties)

  5. USB cable clamp (Type C) x 1 set (1 clip and 1 tie)

  6. DC Power connector x 1

Product Revision and QR Code

You can identify the product version (PV) and the software version (SV) from the product label.

You can also check the contents of this manual by using the QR code on the product label. Confirm the location of the QR code below and refer to the manual.

  1. This mark indicates that you can refer to wiring requirements in this manual by using the QR code. Refer to Wiring the Power Supply.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.