EIO0000005081.01

12-inch and 15-inch

Front
A. Front USB cover
B. USB 2.0 (Type A)*1
C. USB 2.0 (micro-B) (this interface is unavailable.)
D. Status LED

*1 By default, the front USB is disabled. To enable, set in the Launcher.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.