EIO0000005081.01

Periodic Check Points

Operation Environment

When this product is inside a panel, the ambient environment refers to the interior of the panel.

Electrical Specifications

  • Is the input voltage appropriate? Refer to Electrical Specifications.

  • Are all power cords and cables connected properly? Are there any loose cables?

  • Are all installation fasteners holding the unit securely?

  • Are there scratches or traces of dirt on the installation gasket?

Unit Disposal

When disposing this product, dispose it in a manner appropriate to, and in accordance with, your country's industrial machinery disposal/recycling standards.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.