EIO0000005081.01

4G Cellular

Package Contents

  1. 4G M.2 card

  2. Heat sink pad

  3. M3 screw x 3

  4. 4G cellular module bracket

  5. M.2 screw x 1

  6. Antenna x 2

NOTE:
  • Use the interface unit and SIM card that match the frequency in your country.

  • Use this product in accordance with the laws, regulations and standards of your country.

  • This product/accessory has not obtained standards or certifications related to radio frequency. Please obtain if required by the standards and certifications in your country.

  • The data communication is to be set up with Windows standard settings. Refer to Cellular.

Specifications

Product number

HMIYP6M24GW

SIM card type

micro SIM 3FF, 12 x 15 mm

M.2 Key ID

Key B


4G

Standard

3GPP Release 12, LTE-FDD, LTE-TDD

Band

LTE-FDD: B1, B2, B3, B4, B5, B7, B8, B12, B13, B14, B17, B18, B19, B20, B25, B26, B28, B29, B30, B32, B66, B71

LTE-TDD: B34, B38, B39, B40, B41, B42, B43, B46, B48

Link speed

LTE Cat.6


3G

Standard

3GPP Release 9, DC-HSDPA, HSPA+, HSDPA, HSUPA, W-CDMA

Band

B1, B2, B3, B4, B5, B6, B8, B19

Link speed

Max.42 Mbps (DC-HSDPA, DL)

Max.5.76 Mbps (HSUPA, UL)

NOTE: 2G communication (GSM) is not available.

Antenna size

Attaching the 4G Cellular Module and SIM card

CAUTION
LOSS OF COMMUNICATION
Do not put excessive stress on the communication ports of all connections.
Failure to follow these instructions can result in injury or equipment damage.
  1. Disconnect the power supply from the Box Module.

  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.

  3. Remove 3 screws on the front side of the Box Module.

  4. Remove the optional interface cover.

  5. Put the heat sink pad on the board.

  6. Insert the M.2 screw on the slot in 4G M.2 card.

  7. Insert the 4G M.2 card in the slot on the product.

  8. Push the 4G M.2 card from above and secure it with the M.2 screw.

    NOTE:
    • Using a Phillips screwdriver #1 is recommended.

    • The necessary torque is 0.2 N•m (1.77 lb-in).

  9. Slide the cover of the SIM card holder in the direction of the arrow to open it.

  10. Insert the SIM card into the slot and close and slide the cover in the direction of the arrow to lock.

  11. Insert the 4G module bracket.

  12. As shown below, plug the antenna cable connector securely to the connector on the 4G M.2 card. Looking from above the interface, plug the black cable connector to the connector on the left side on the 4G M.2 card, and the white cable connector to the connector on the right side.

  13. Fix the 4G module bracket on the product and tighten with M3 screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
  14. Place the optional interface cover on the Box Module.

  15. Secure the optional interface cover on the Box Module with the screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
  16. Attach the antenna only after mounting the product on the panel.

    Do not block the antenna area with your hand, body or other objects. It may cause interference in communications.

    You can change the direction of antennas, up, down, left and right.

    You can attach the antenna to the outside of the panel using the following optional cable.

    4G Cellular extended antenna cable (3 m): HMIYP6CB4G3M

    When the optional cable is used, the dimensions of the panel opening are as follows.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.