EIO0000005081.01

Basic Box

Front

Right

Bottom

A. Optional module interface

J. USB 3.1 Gen1 (Type A)

B. SD slot screw

K. Ethernet interface (ETH1)

C. Status LED

L. Ethernet interface (ETH2)

D. Storage access LED

M. USB 3.1 Gen1 (Type C)

E. Error LED

N. DisplayPort

F. SD slot cover

O. Serial interface (RS-232C/422/485, non-isolated) (COM1) *1

G. FG terminal ()

P. Serial interface (RS-232C/422/485, non-isolated) (COM2) *1

H. DC power connector

Q. Reset button

I. USB 3.1 Gen1 (Type A)

R. Power button *2

*1 For the settings of the serial ports on Box Module, refer to Settings of Serial Interfaces on Box Module.

*2 The power button in Windows Power Options is set to Shut down by default. The following options are available for the power button. Select an option suitable for your usage environment.

  • Do nothing
  • Sleep
  • Hibernate
  • Shut down (default)
  • Turn off the display

NOTE: The marking attached on the rear face of the Box Module () indicates that you need to refer to the manual.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.