EIO0000005081.01

Installing/Replacing DIMM

  1. Disconnect the power supply from the Box Module.

  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.

  3. Remove 12 screws on the rear side of the Box Module and pull out the rear cover.

  4. If DIMM is already inserted, remove the lock from the DIMM on the product.

  5. Remove the DIMM.

  6. Insert the DIMM on the product.

  7. Push the DIMM on the product and then the DIMM is locked.

  8. Place the rear cover of the Box Module and tighten with screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.