EIO0000005081.01

Removing the Display Module from the Box Module

CAUTION
RISK OF INJURY
Do not drop the Box Module when you remove it from the Panel Type.
  • Hold this product in place after removing the screws.
  • Use both hands.
Failure to follow these instructions can result in injury or equipment damage.
  1. Place the Panel Type on a clean and level surface with the screen facing down.
  2. Remove the screws (4 pieces) on the rear face, then remove the Box Module.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.