EIO0000005081.01

Touch Mode

The following three modes are available to support your usage environment. Select the mode according to your usage environment.

NOTE: This function is available only on the models with a projected capacitive touch panel.
Standard Mode Factory default. Suitable for touch operations using your finger.
Water Detection Mode Mode where touch input becomes disabled when there are liquids, such as drops of water, on the screen. Suitable to prevent touch panel mis-operation due to liquids on the screen. After wiping the liquid or other foreign substance from the screen, touch input becomes enabled in about 2 seconds.
Glove Mode Mode suitable for use with gloves, such as rubber gloves.
NOTE:
  • Depending on the type of glove, operation may not be possible.

  • Because touch sensitivity is increased in this mode, it is more susceptible to environmental noise.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.