EIO0000005081.01

Ethernet (GbE IEEE1588)

Package Contents

  1. Ethernet module bracket

  2. M.2 screw x 1

  3. Ethernet M.2 card

  4. M3 screw x 3

Specifications

NOTE: Install the latest version of the driver before using this interface. You can download the latest driver from our website.
www.se.com/ww/en/download

Product number

HMIYP6M2ETH

Connector

Modular jack (RJ-45) x 1

Standard

IEEE1588,  IEEE802.3, 10 BASE-T/100BASE-TX/1000 BASE-T, Wake-on-LAN (WOL) supported*1

Maximum communication distance

100 m (328.1 ft)

M.2 Key ID

Key B

*1 When the status is S4 (hybrid shutdown), Wake-on-LAN is unavailable.

CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
Failure to follow these instructions can result in injury or equipment damage.

LED Indications

  1. ACT

  2. LINK

Color

Indicator

Description

Green (Active)

ON

Data transmission is available

Flashing

Data transmission in progress

OFF

No connection or data transmission error

Green (Link)

ON

Data transmission is available.

OFF

No connection or data transmission error

Installing Ethernet Module

  1. Disconnect the power supply from the Box Module.

  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.

  3. Remove 3 screws on the front side of the Box Module.

  4. Remove the optional interface cover.

  5. Insert the M.2 screw on the slot in the Ethernet M.2 card.

  6. Insert the Ethernet M.2 card in the slot on the product diagonally.

  7. Push the Ethernet M.2 card down and tighten with M.2 screw.

    NOTE:
    • Using a Phillips screwdriver #1 is recommended.

    • The necessary torque is 0.2 N•m (1.77 lb-in).

  8. Place the Ethernet module bracket on the product.

  9. Connect the port cable of the Ethernet module bracket to the socket on the Ethernet M.2 card.

  10. Secure the Ethernet module bracket on the product with M3 screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
  11. Place the optional interface cover on the Box Module.

  12. Secure the optional interface cover on the Box Module with the screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.