EIO0000005081.01

Installing M.2 SSD for Secondary Storage

When installing the M.2 SSD, the optional M.2 cooling kit is required. Purchase and install using the following steps.

M.2 cooling kit for Basic Box: HMIYP6HSM2B

  1. Heat sink pad

  2. Screw for M.2 SSD

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. This product is designed to use 12 to 24 Vdc. Always check whether your device is DC powered before applying power.
Failure to follow these instructions will result in death or serious injury.
CAUTION
STORAGE DEVICE DAMAGE AND DATA LOSS
  • Remove all power before making any contact with an installed storage device.
  • Use only our optional storage devices for this product.
  • Make sure you regularly back up the data since storage devices have a life span and accidental data loss can occur at any time.
  • Confirm the storage device is correctly oriented before insertion.
  • Do not bend, drop, or strike the storage device.
  • Do not touch inside the storage device or its connectors.
  • Do not disassemble or modify the storage device.
  • Keep the storage device dry.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
ELECTROSTATIC DISCHARGE
Take the necessary protective measures against electrostatic discharge before attempting to remove the cover.
Failure to follow these instructions can result in equipment damage.
NOTICE
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Keep the M2 cooling kit ready.

  2. Disconnect the power supply from the Box Module.

  3. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.

  4. Remove 3 screws on the front side of the Box Module.

  5. Remove the optional interface cover.

  6. Peel off the protective film from the top surface and bottom surface of the heat sink pad.

  7. Place the heat sink pad on the board.

  8. Insert the M.2 screw in the M.2 SSD card.

  9. Insert the M.2 SSD card in the slot.

  10. Secure the M.2 SSD card with the M.2 screw.

    NOTE:
    • Using a Phillips screwdriver #1 is recommended.

    • The necessary torque is 0.2 N•m (1.77 lb-in).

  11. Place the optional interface cover and tighten with screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.