EIO0000005081.01

Wall Mounting

Install the product to the panel or wall with M4 screws (4 pieces).

NOTE:
  • The necessary torque is 1.5 N•m (13.3 lb-in).

  • With this installation method, the interface side (the bottom of the product) must be facing downward.

  • To prevent abnormally high temperatures from occurring inside the product, mount the product completely vertically.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.