EIO0000005081.01

Removing the SD Card

If you remove the SD Card while it is in use, you risk corrupting your data. Before removing the SD Card from this product, stop all operations on the SD Card.

  1. Remove the SD card using Windows "Safely Remove Hardware and Eject Media".

  2. Remove the screw indicated on the front side the Box Module.

  3. Open the SD slot cover.

  4. Push the SD Card once to release.

    NOTE:

    After using the SD Card, store the SD Card in its case or other safe location.

  5. Pull out the card.

  6. Close the SD slot cover.

  7. Secure the SD slot cover with the screw removed in step 2.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.