EIO0000005081.01

Uninstallation

When uninstalling, you need to uninstall the following two applications.

  • Trellix Solidifier

  • Trellix Installer

Steps for uninstalling is as follows.

  1. Select the Settings button.
  2. In Apps & features, select Trellix Solidifier.
  3. Select Uninstall.
  4. Follow the same steps and select Trellix_Installer, and then Uninstall.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.