EIO0000005081.01

RS-232C isolated x 2

Package Contents

  1. RS–232C module bracket

  2. M3 screw x 3

  3. M.2 screw x 1

  4. RS-232C M.2 card

  5. Insulation sheet

Specifications

  1. COM4

  2. COM3

Product number

HMIYP6M2R23P2

Asynchronous transmission

RS-232C (isolated) x 2

Data length

7 or 8 bits

Stop bit

1 or 2 bits

Parity

None, odd or even

Flow control

Hardware flow control: RTS/CTS

Software flow control: Xon/Xoff

Data transmission speed

2,400...115,200 bps

Connector

D-Sub 9 pin (plug)

M.2 Key ID

Key B

The serial interface is isolated. The SG (signal ground) and FG (frame ground) terminals are not connected inside this product. When the serial interface connector is D-Sub, connect the FG wire to the shell.

DANGER
ELECTRIC SHOCK AND FIRE
When using the SG terminal to connect an external device to this product:
  • Verify that a ground loop is not created when you set up the system.
  • Connect the SG terminal to remote equipment when the external device is not isolated.
  • Connect the SG terminal to a known reliable ground connection to reduce the risk of damaging the circuit.
Failure to follow these instructions will result in death or serious injury.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use a D-Sub 9 pin connector that has jack screws.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

Pin Assignment

D-Sub 9 pin plug connector

Module side:

Pin No.

RS-232C

Signal name

Direction

Description

1

CD

Input

Carrier detect

2

RD (RXD)

Input

Receive data

3

SD (TXD)

Output

Send data

4

ER (DTR)

Output

Data terminal ready

5

SG

-

Signal ground (isolated)

6

DR (DSR)

Input

Data set ready

7

RS (RTS)

Output

Request to send

8

CS (CTS)

Input

Send possible

9

CI (RI)

Input

Called status display

Shell

FG

-

Frame ground

Recommended jack screw is #4-40 (UNC).

Installing RS-232C Module

  1. Disconnect the power supply from the Box Module.

  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.

  3. Remove 3 screws on the front side of the Box Module.

  4. Remove the optional interface cover.

  5. Put the insulation sheet on the board.

  6. Insert the M.2 screw on the slot in RS-232C M.2 card.

  7. Insert the RS-232C M.2 card in the slot on the product.

  8. Push the RS-232C M.2 card and tighten with M.2 screw.

    NOTE:
    • Using a Phillips screwdriver #1 is recommended.

    • The necessary torque is 0.2 N•m (1.77 lb-in).

  9. Connect the port cable of the RS-232C module bracket to the socket on the RS-232C M.2 card.

  10. Fix the RS-232C module bracket on the product and tighten with M3 screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
  11. Place the optional interface cover on the Box Module.

  12. Secure the optional interface cover on the Box Module with the screws.

    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.