EIO0000005081.01

Display Module LED Indications

Status LED

Color State Description
Green ON In operation
Flashing Screen is turned off.
Orange ON*1 S3, S4, S4 (hybrid shutdown)*2, S5
Flashing Either software starting up or internal error*3
Orange/Red Alternating System monitor error
OFF Power is off.

*1 Immediately after hibernation or when HORM is enabled, the LED on the Display Module turns orange right away, but turn off the power only after confirming the status LED on the Box Module has turned red.

*2 S4 (hybrid shutdown) is S5 when Windows® fast startup is enabled.

*3 Restart if flashing orange continues.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.