Class 9999 / Refer to Catalog 9999CT9701

Isolated Alarm Contacts For Melting Alloy Overload Relays

Type SO4

Isolated overload relay alarm contacts are available factory-installed or in kit form for field installation in NEMA Size 00–6 Type S[1] starters, and Class 9065 Type SE melting alloy overload relays. NEMA Size 7 Type S devices use a solid­state overload relay which has isolated alarm contacts as a standard feature. The alarm contacts allow the starter to be used in applications that require isolated contacts, such as inputs to a computer.

Class 9999 Types SO4 and SO5 modules are interchangeable with the standard module (Class 9998 Type SO1) and can be installed on starters already in service. The case is made of clear plastic (polycarbonate) to allow for visual inspection of contacts.

Contact Unit for Melting Alloy Overload Relays, Class 9999

Magnetic Starter

Parts Kit Description

Catalog Number

NEMA
Size

Type

00-6 [1]

SA-SH

N.O. Isolated Alarm Contact Plus
Standard N.C. Overload Contact

9999SO4

N.C. Isolated Alarm Contact Plus
Standard N.C. Overload Contact

9999SO5

Solid Neutral

The Class 9999 Type SN kit can be used on Class 8903 Type S lighting contactors and other controllers where field addition of a solid neutral is required. Each kit has lugs suitable for both copper and aluminum wire, and mounts with two screws.

Solid Neutral Selection

Number of
Lugs

Wire Capacity
Per Lug (Cu/Al)

Class 9999

Type

4

14–2/0

SN1

3

one 4–600 MCM or
two 1/0–250 MCM

SN2

3 (Dual)

two 2–600 MCM

2 (Dual)

two 6–350 MCM

SN4

Tie Point Terminal Block

Tie Point Terminal Block

How to Order

To Order Specify:

Catalog Number

  • Class Number

  • Type Number

Class

Type

9999

SO4

The tie point terminal block provides easy wiring of a Hand-Off-Auto selector switch or Start-Stop push buttons with separate control. The T7 terminal block requires no panel space. It simply snaps on Sizes 00–4 Type S contactors and starters by two tabs and is secured to the left hand coil terminal.

Tie Point Terminal Block Selection

Magnetic
Contactor or Starter

Class 9999
Type

NEMA Size

Type

00–4

SA-SF

T7

Footnotes

  1. Isolated alarm contacts cannot be added in the field to the Size 5 Type S starter. Current transers and a Size 1 overload block must be used. For factory installation specify Form Y342.
Feedback