8536IB1904EN-04

Dual-Channel Architecture (ISO 13849)

TeSys island is applicable to dual-channel architectures in which a single detected fault (including common-mode faults) does not lead to the loss of the safety function.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.