8536IB1904EN-04

SIL Stop, Stop Category 1, Wiring Category 3/4

Example: SIL Stop, Stop Category 1, Wiring Category 3/4 *

Legend for Example: SIL Stop, Stop Category 1, Wiring Category 3/4

Parallel link

S2 Start Button

Reversing link

Input

Power supply

Start

Flat cable connector

Extension

SIL interface Module (SIM)

Controlled stop

Preventa XPS-UAF Module

Stop Category 1

Emergency stop push button (S1)

   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.