8536IB1904EN-04

SIL Starter

The following data help define the level of performance for SIL* starters.

B10: 1,000,000

% of dangerous failures*: 73%

B10d: 1,369,863

Assuming number of operations = 131,400 cycles/year (average of 15 cycles/hour)

The calculated values of the SIL starter are provided in the following tables:

SIL Starter in Single Channel

Wiring Category*

SFF

HFT

MTTFd (years)

DC

Category 1

27%

0

100 years

Not relevant

Category 2 – Direct monitoring

90%

0

100 years

≥ 90%

SIL Starter in Dual Channel

Wiring Category SFF HFT MTTFd (years) DC

Category 3

27%

0

100 years

≥ 90%

Category 4

90%

0

100 years

≥ 99%

The relation between PFHd and PFD of the SIL starters, depending on the architecture and the test interval, is given in the following table:

SIL Starters — PFHd and PFD

Wiring Category

PFH (IEC 61508)

PFD (IEC 61508)
Ti=10 years*

PFD (IEC 61508)
Ti=5 years*

Category 1

1.10E-06

4.80E-02

4.82E-03

Category 2 – Direct monitoring

1.10E-06

4.82E-03

5.06E-04

Category 3

4.5E-09

1.30E-04

Category 4

2.5E-10

2.5E-06

Architectural requirements defined in IEC 61508-2 Table 3 and EN 62061 Table 5 are met for levels up to SIL 2.

A Category 2 architecture is needed to meet SIL 2 architectural constraints (accomplished using direct monitoring Mirror In/Mirror Out).

NOTE: The fault detection and specified fault reaction must be performed before the hazardous situation addressed by the safety-related control function can occur.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.