8536IB1904EN-04

SIL Interface Module

Calculated Values of the SIL * Interface Module (SIM)

Architecture

SIM

PFH*

PFD*

SFF*

HFT*

MTTFd (years)

DC*

Wiring Category 1*

2.10 – 10

2.10 – 5

>90%

1

17,459

Not relevant

Wiring Category 2

>99%

90%

Wiring Category 3

>99%

90%

Wiring Category 4

99%

99%

NOTE: PFD and PFH values are calculated with the following:
  • Test Interval = 20 years

  • MTTR*=MRT* = 24 hours

Architectural requirements defined in IEC 61508-2 Table 3 and EN 62061 Table 5 are met for levels up to SIL 3.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.