8536IB1904EN-04

EN ISO 13849 Standard

This European Standard specifies the validation process, including hazard analysis, risk assessment, and testing, for the safety functions and categories for the safety-related parts of control systems. Descriptions of the safety functions and the requirements for the categories are given in ISO 13849-1, which covers the general principles for design. Some requirements for validation are general and some are specific to the technology used. EN ISO 13849-2 also specifies the conditions under which the validation by testing of the safety-related parts of control systems should be carried out.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.