8536IB1904EN-04

SIL Stop, Stop Category 0, Wiring Category 2

Example: SIL Stop, Stop Category 0, Wiring Category 2 *

Legend for Example: SIL Stop, Stop Category 0, Wiring Category 2

Mechanical interlock

Emergency stop push button (S1)

Parallel link

Preventa XPS-UAF Module

Reversing link

Start button (S2)

Power supply

Input

Flat cable connector

Start

SIL interface module (SIM)

Extension

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.