8536IB1904EN-04

Operating Conditions

TeSys island is designed to durably sustain the following conditions. Other conditions may apply to specific modules as described in their data sheet document, available on www.se.com/tesys-island .

  • 40 °C (104 °F) ambient temperature

  • 400 or 480 V motor

  • 50% humidity

  • 80% load

  • Horizontal mounting orientation

  • All inputs activated

  • All outputs activated

  • 24 hours/day, 365 days/year run time

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.