8536IB1904EN-04

SIL Stop, Stop Category 0, Wiring Category 3/4

Example: SIL Stop, Stop Category 0, Wiring Category 3/4 *

Legend for Example: SIL Stop, Stop Category 0, Wiring Category 3/4

Power supply

Start button (S2)

Emergency stop push button (S1)

Input

Flat cable connector

Start

SIL interface module (SIM)

Extension

Preventa XPS-UAF Module

   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.