8536IB1904EN-04

Low Switching Frequency (< 15 cycles per hour)

In low switching frequency, the SIL * Stop and the operational on/off control functions can be achieved together with a SIL avatar.

Example Avatar with SIL Starter

Low Switching Frequency — Operational and Safety Functions

SIL Avatar

Module 1

Module 2

Module 3

Module 4

Module 5

Switch - SIL Stop, W. Cat 1/2*

SIL Starter

SIM

Switch - SIL Stop, W. Cat 3/4*

SIL Starter

SIL Starter

SIM

Motor One Direction - SIL Stop, W. Cat 1/2

SIL Starter

SIM

Motor One Directions - SIL Stop, W. Cat 3/4

SIL Starter

SIL Starter

SIM

Motor Two Directions - SIL Stop, W. Cat 1/2

SIL Starter

SIL Starter

SIM

Motor Two Directions - SIL Stop, W. Cat 3/4

SIL Starter

SIL Starter

SIL Starter

SIM

Motor Two Speeds - SIL Stop, W. Cat 1/2

SIL Starter

SIL Starter

SIM

Motor Two Speeds - SIL Stop, W. Cat 3/4

SIL Starter

SIL Starter

SIL Starter

SIM

Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

SIL Starter

SIL Starter

SIM

Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

SIL Starter

SIL Starter

SIL Starter

SIL Starter

SIM

Conveyor One Direction - SIL Stop, W. Cat 1/2

SIL Starter

SIM

Conveyor Two Directions - SIL Stop, W. Cat 1/2

SIL Starter

SIL Starter

SIM

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.