8536IB1904EN-04

Architectural Requirements for Wiring Category 1

Designated architecture for Category 1 is defined in EN ISO 13849-1, 6.2.4.

Designated architecture for Category 1 (EN ISO 13849-1)

I: input device

L: logic

O: output device

im: interconnecting means

SRP/CS, the safety-related part of the control system, of Wiring Category 1 must be designed and constructed using well-tried components.

A “well-tried component” for a safety-related application is a component which has been either:

  • widely used in the past with successful results in similar applications, or

  • made and verified using principles which demonstrate its suitability and reliability for safety-related applications.

There is no diagnostic coverage (DCavg = none) within Category 1 systems.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.