8536IB1904EN-04

Performance Level (PL)

The standard IEC 13849-1 defines five performance levels (PL) for safety functions.

Level a is the lowest level and e is the highest.

Five levels (a, b, c, d, and e) correspond to different values of average probability of dangerous failure* per hour.

Performance Level

Probability of a Dangerous Failure* per Hour

e

≥ 10-8 to < 10-7

d

≥ 10-7 to < 10-6

c

≥ 10-6 to < 3 x 10-6

b

≥ 3 x 10-6 to < 10-5

a

≥ 10-5 to < 10-4

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.