8536IB1904EN-04

SIL Avatars

SIL* avatars available for SIL Stop functions are:

  • Switch - SIL Stop, W. Cat 1/2

  • Switch - SIL Stop, W. Cat 3/4

  • Motor One Direction - SIL Stop, W. Cat 1/2

  • Motor One Direction - SIL Stop, W. Cat 3/4

  • Motor Two Directions - SIL Stop, W. Cat 1/2

  • Motor Two Directions - SIL Stop, W. Cat 3/4

  • Motor Two Speeds - SIL Stop, W. Cat 1/2

  • Motor Two Speeds - SIL Stop, W. Cat 3/4

  • Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2

  • Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

  • Conveyor One Direction - SIL Stop, W. Cat 1/2

  • Conveyor Two Directions - SIL Stop, W. Cat 3/4

SIL avatars consist of specific hardware devices, including SIL starters, standard starters, and the required SIL interface module that manages the SIL group that the SIL avatars are assigned to.

NOTE: SIL avatars are designed for applications with a low frequency of operational commands—below a yearly average of 15 start/stop cycles per hour.

SIL Starter

Standard Starter

SIL Interface Module

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.