8536IB1904EN-04

SIL Stop, Stop Category 1, Wiring Category 2

Example: SIL Stop, Stop Category 1, Wiring Category 2 *

Legend for Example: SIL Stop, Stop Category 1, Wiring Category 2

Mechanical interlock

Input

Parallel link

Start

Reversing link

Extension

Flat cable connector

Controlled stop

SIL interface module (SIM)

Stop Category 1

Power supply

Upstream circuit breaker

Emergency stop push button (S1)

PLC

S2 Start Button

Bus coupler

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.