8536IB1904EN-04

SIL Avatar Wiring

The wiring diagrams in this section are for the SIL* avatars. The following table is a legend for the diagrams in this section.

Legend for Wiring Diagrams

Mechanical interlock

Parallel link

Reversing link

Electrical circuit

Switch - SIL Stop, W. Cat 1/2 *

Motor One Direction - SIL Stop, W. Cat 1/2

Motor Two Directions - SIL Stop, W. Cat 1/2

Motor Two Speeds - SIL Stop, W. Cat 1/2

Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2

Switch - SIL Stop, W. Cat 3/4 *

Motor One Direction - SIL Stop, W. Cat 3/4

Motor Two Directions - SIL Stop, W. Cat 3/4

Motor Two Speeds — SIL Stop, W. Cat 3/4

Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

Conveyor One Direction - SIL Stop, W. Cat 1/2

Conveyor Two Directions - SIL Stop, W. Cat 1/2

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.