8536IB1904EN-04

Average Frequency of Dangerous Failure [h-1] (PFH). (Dangerous failure as defined in IEC 61508-4)

To maintain the safety function, the IEC 61508 standard requires various levels of measures for avoiding and controlling detected errors, depending on the required SIL*.

All components of a safety function must be subjected to a probability assessment to evaluate the effectiveness of the measures implemented for controlling detected faults.

This assessment determined the PFH (Average Frequency of Dangerous Failure* [h-1]) for a safety-related system. This is the probability per hour that a safety-related system fails in a hazardous manner and the safety function cannot be correctly executed.

Depending on the SIL, the PFH must not exceed certain values for the entire safety-related system.

The individual PFH values of a function chain are added. The result must not exceed the maximum value specified in the standard.

Safety Integrity Level

Average Frequency of Dangerous Failure* [h-1] (PFH) at High Demand or Continuous Demand

4

10-9 ≤ — < 10-8

3

10-8 ≤ — < 10-7

2

10-7 ≤ — < 10-6

1

10-6 ≤ — < 10-5

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.