8536IB1904EN-04

Reliability Data

Safety Function Standard Reference

The SIL* Stop function has priority over a stop triggered for operational reasons (EN ISO 13849-1, 5.2.1).

The performance level depends on the wiring category*, the MTTFd, and the DCavg.

The following diagram shows the positioning of TeSys™ island according to the category requirement.

TeSys island Positioning by Category Requirement

Simplified Procedure for Evaluating PL Achieved by Safety-Related Parts of Control Systems (SRP/CS)

Category

B

1

2

2

3

3

4

DCavg

none

none

low

medium

low

medium

high

MTTFd of each channel

Low

a

Not covered

a

b

b

c

Not covered

Medium

b

Not covered

b

c

c

d

Not covered

High

Not covered

c

v

d

d

d

e

According to TeSys island architecture and wiring category, the key indicators (DCavg, MTTFd, PL) for TeSys island comply with the values shown in the table below.

Values of Key Indicators for Single and Dual Channel Architectures

TeSys island system architecture

Category

Single fault tolerance*

DCavg

MTTFd of each channel

Targeted PL

Single channel

1

No

None

High (≥ 30 years)

c

2

No

Low (≥ 60%) to medium (≥ 90%)

Low (≥ 3 years) to high (≥ 30 years)

c, d

Dual channel

3

Yes

c, d, e

4

Yes

High (≥ 99%)

High (≥ 30 years)

e

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.