8536IB1904EN-04

Acceptance Test

The system integrator/machine manufacturer must perform an acceptance test of the safety function to verify and document the correct functionality of the safety function. The system integrator/machine manufacturer thereby certifies to have tested the effectiveness of the safety functions used. The acceptance test must be performed based on the hazard analysis and risk assessment. In case of low demand mode with category 4, the safety function should be tested at least once per month. All applicable standards and regulations must be followed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.