8536IB1904EN-04

SIL Starters Contact Status

The status of the SIL* starters belonging to a SIL group is reported via the SIM Mirror In/Out connections. This allows the implementation of Wiring Category 2* architectures where the mirror contacts are connected to the Preventa XPS module (or equivalent). These configurations provide direct monitoring capabilities of electromechanical devices by a mechanically linked contact element, which gives diagnostic coverage up to 99%. Refer to EN ISO 13849-1, Table E.1 – Estimates for diagnostic coverage (DC).

SIL Starter Contact Status

SIL Group Status

Mirror In/Out Status

All SIL Starters are open

Mirror In/Out contact is closed

At least one SIL Starter is closed

Mirror In/Out contact is open

TeSys island unpowered, or fault detected by the safety function

Mirror In/Out contact is open

SIM to Preventa Module XPS-AF Wiring

External start conditions (ESC)

Start button (S2)

Emergency stop push button (S1)

Power supply

Preventa XPS-UAF Module

Input

SIM mirror out

Start

SIM mirror in

Extension

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.