8536IB1904EN-04

SIL Group

A SIL* group is made up of one or more SIL avatars, all assigned to a single SIL interface module. All SIL avatars in the SIL group react to a single SIL Stop Command. The SIL interface module is always installed to the right of the last SIL starter included in the SIL group (far side of the bus coupler).

An island may include several SIL groups.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.