8536IB1904EN-04

SIL Stop, Stop Category 0, Wiring Category 1 Configuration

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 1 according to ISO 13849. Stop Category 0 according to EN/IEC 60204-1.

The SIL Stop of the motor is directly controlled by the opening of the contact of the emergency stop push button.

SIL Stop

Avatar A1

Wiring Category 1, Stop Category 0

SIL Group 1

PLC

Motor

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.