8536IB1904EN-04

EN/IEC 60204-1 Standard

Stop Category 0 is defined as a function “stopping by immediate removal of power to the machine actuators (i.e. an uncontrolled stop).”

Stop Category 1 is defined as “a controlled stop with power available to the machine actuators to achieve the stop and then removal of power when the stop is achieved.”

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.