8536IB1904EN-04

Hardware Fault Tolerance (HFT) and Safe Failure Fraction (SFF)

Depending on the SIL * for the safety-related system, the IEC 61508 standard requires a specific hardware fault tolerance (HFT) in connection with a specific proportion of safe failures, shown as Safe Failure Fraction (SFF).

The HFT is the ability of a system to execute the required safety function in spite of the presence of one or more hardware faults.

The SFF of a system is defined as the ratio of the rate of safe failures to the total failure rate of the system.

According to IEC 61508, the maximum achievable SIL of a system is partly determined by the HFT and the SFF of the system.

These types are specified on the basis of criteria which the standard defines for the safety-related elements.

SFF

HFT Type A Subsystem

HFT Type B Subsystem

 

0

1

2

0

1

2

< 60%

SIL 1

SIL 2

SIL 3

SIL 1

SIL 2

60% – < 90%

SIL 2

SIL 3

SIL 4

SIL 1

SIL 2

SIL 3

90% – < 99 %

SIL 3

SIL 4

SIL 4

SIL 2

SIL 3

SIL 4

≥ 99%

SIL 3

SIL 4

SIL 4

SIL 3

SIL 4

SIL 4

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.