8536IB1904EN-04

SIL Interface Module

The TeSys™ island SIL* interface module (SIM) is an accessory module required to enable the Functional Safety feature of the island.

The SIL Stop function is achieved by pure electromechanical means without any digital communication or bus coupler involvement.

The SIM:

  • interfaces with an external Preventa™ XPS module (or equivalent)

  • commands the stop function of its SIL group

  • exchanges operational data with the bus coupler

  • reports operational information through front face LEDs

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.