8536IB1904EN-04

SIL Stop, Stop Category 1, Wiring Category 2 Configuration

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 2 according to ISO 13849. Stop Category 1 according to EN/IEC 60204-1.

Stop Category 1 is defined as “a controlled stop with power available to the machine actuators to achieve the stop and then removal of power when the stop is achieved.”

When the emergency stop is triggered, the stop command is first sent to an external device (for example, a PLC or a drive). In this way, the process is stopped in a controlled manner rather than by immediate power removal. After a pre-defined time, the SIL Stop Command is then sent to the SIM to de-energize loads on the SIL avatars in the associated SIL group.

The recommended setup is to use a PLC to help ensure that the process is correctly stopped before the SIL Stop occurs.

The stop command can be routed directly to a digital input of the PLC, or to a TeSys™ island Digital I/O Module avatar, using one of its digital inputs read by the PLC. Upon receiving a stop command input, the PLC initiates a controlled stop by issuing an operational stop command to the targeted TeSys island avatar.

Stop Command

Avatar A1

Wiring Category 2, Stop Category 1

SIL Group 1

Controlled Stop Category 1 command

Motor

PLC

Uncontrolled stop

Operational stop command

Example: Motor Two Directions - SIL Stop, W. Cat 1/2 — Stop Category 1, Wiring Category 2 Configuration

Legend for Example: Motor Two Directions - SIL Stop, W. Cat 1/2 — Stop Category 1, Wiring Category 2 Configuration

Mechanical interlock

Controlled stop

Parallel link

Stop Category 1

Reversing link

Upstream circuit breaker

Flat cable connector

PLC

SIL interface module (SIM)

Bus coupler

Preventa XPS-UAF Module

Input

Emergency stop push button

Start

S2 Start Button

Extension

Power supply

   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.