8536IB1904EN-04

Single-Channel Architecture (ISO 13849)

TeSys island is applicable to single-channel architectures in which a detected fault can lead to the loss of the safety function.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.